Get or Update a SIRC File

Instrument:
N1000A
Flex Apps:
FlexDCA
Package License:
L-RND

If no SIRC calibration is loaded for the module, the following message is display at the top of the System Impulse Response Correction Setup dialog. If this happens, click the expand button at the bottom of the dialog to view the setting shown below.

To select the source of the SIRC data to import, select one of the following sources for the file locations:

Local Drive
Select to locate a calibration file this is located on the DCA-X or the PC, depending on whether FlexDCA is running on a PC or is embedded. Click Browse to locate the file.
Remote DCA
This selection is displayed whenever FlexDCA is remotely controlling a DCA-X. A calibration file is used that is located on the DCA-X. Click Check for Updates Now to automatically select and use the data file. The file is expected to be in the default /SIRC Calibration folder this is shown in the picture that is located at the end of this topic.

If a dark calibration is performed while SIRC data is loaded, the SIRC data is temporarily turned off during the dark calibration.

Modification of the SIRC file or use of this data with any other module or product or for any other purpose is prohibited, may provide incorrect measurement results, and will void the warranty.