Lowest Symbol Results
Instrument:
N1000A-PLK
N109X-PLK
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
NRZ
Package License:
L-RND
Locates the symbol with the Lowest amplitude for the specified logic level. This measurement can only be viewed in the results table by sending the :MEASure:AMPLitude:LSYMbol command. The default level is 0. To specify a different logic level, use the :MEASure:AMPLitude:LSYMbol:LEVel command. For NRZ signa,s you can select levels 0 and 1. For PAM4 signals, you can select levels 0, 1, 2 and 3.
More Information
SCPI Command
:MEASure:AMPLitude:LSYMbol