UN Result

Instrument:
N1000A-PLK
N109X-PLK
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
NRZ
Package License:
L-RND

Click the Measurement (Meas) toolbar's Uncorrelated Noise to activate Jitter mode's Uncorrelated Noise (UN) measurement which is the total of these values:

  • Random Noise (RN) that is unpredictable and not data related, and
  • Asynchronous Periodic Noise (APN) that is periodic noise that is uncorrelated to the symbol rate.

The measurement result is shown in the Amplitude Components Tree.

More Information

SCPI Command

:MEASure:AMPLitude:UN