TDR Mode (Amplitude Toolbar)
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Use the Amplitude measurement toolbar to perform the measurements listed in this topic's menu. With the exception of Excess Capacitance and Excess Inductance, these measurements use the same algorithm as the corresponding Oscilloscope measurements.
For TDR/TDT measurements, standards may specify the thresholds used to determine the risetime of a discontinuity that is measured on a TDR/TDT waveform. You can specify this threshold ( 10%/90% or 20%/80%) in the Thresholds tab of the Configure Measurements dialog.