TDR Mode (Time Toolbar)
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Use the Time measurement toolbars to perform the measurements listed in this topic's menu. For TDR/TDT measurements, standards may specify the thresholds used to determine the risetime of a discontinuity that is measured on a TDR/TDT waveform. You can specify this threshold ( 10%/90% or 20%/80%) in the Thresholds tab of the Configure Measurements dialog. These measurements use the same algorithm as the corresponding Oscilloscope measurements.