Minimum
Instrument:
                                                N1000A
                                            Flex Apps:
                                                FlexDCA
                                            Meas. mode:
                                                TDR
                                            Waveform type:
                                                T-Parameter
                                                S-Parameter
                                            
                                                 
                                                 Measures the  minimum amplitude of the waveform's displayed power or voltage.  The measurement can  be restricted to a measurement region. A level annotation label is placed at the minimum result. The entire screen is the interval over which the measurement is made. In TDR/TDT mode, the measurement can be performed on any waveform that is displayed in one of the following content windows:
Measures the  minimum amplitude of the waveform's displayed power or voltage.  The measurement can  be restricted to a measurement region. A level annotation label is placed at the minimum result. The entire screen is the interval over which the measurement is made. In TDR/TDT mode, the measurement can be performed on any waveform that is displayed in one of the following content windows:
- Waveform
- Time-Ohms
- Time-Volts
- Time-%
 
                                            Configurable Measurement Parameters
This measurement is not affected by setting in the Configure Base Measurements dialog.
To measure
- Click the toolbar's More buttons to locate the Minimum button.
- Click the button.
- If measurement regions are enabled, the Select Measurement Region, Setting dialog is displayed. Select the area over which the measurement is to be performed: a Region or the Entire Display.
SCPI Command
:MEASure:TDR:VMINimum