Maximum
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Measures the maximum amplitude of the waveform's displayed power or voltage. The measurement can be restricted to a measurement region. A level annotation label is placed at the maximum result. The entire screen is the interval over which the measurement is made. The measurement can be performed on any waveform that is displayed in one of the following content windows:
- Waveform
- Time-Ohms
- Time-Volts
- Time-%

Configurable Measurement Parameters
This measurement is not affected by setting in the Configure Base Measurements dialog.
To measure
- Click the toolbar's Amplitude tab.
- Click the toolbar's More buttons to locate the Maximum button.
- Click the button.
- If measurement regions are enabled, the Select Measurement Region, Setting dialog is displayed. Select the area over which the measurement is to be performed: a Region or the Entire Display.
SCPI Command
:MEASure:TDR:VMAXimum