N1060A

Instrument
N1000A-PTB
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter

Precision Timebase Module Setup

Use the N1060A Precision Timebase Setup dialog to configure and turn on the module's precision timebase. The module has a front-panel port to connect an external clock.

If the dialog displays the message Precision timebase calibration is recommended as shown in the above picture, click the menu commands Tools > Calibrations to locate and perfomr the calibration.

Before entering the data in this dialog, make the required connections as shown in the following figure. When the precision timebase is used, the instrument does not normally use a trigger. The reference clock is connected directly to the module's front-panel Precision Timebase Input.

If pattern lock is turned on or Jitter Mode is used, connect the reference clock to both the module's precision timebase reference clock Input and to the DCA-X's front-panel Trigger Input.

Figure. Setup for N1060A with Pattern Lock or Jitter Mode

Reference Clock Frequency Settings

Select the Reference Clock Frequency by clicking Select From List. This displays a list of standard optical and digital telecommunications rates. This list is also available in the Pattern Lock Setup tab of the Trigger dialog. FlexDCA determines the phase of a data sample within one period.

If pattern lock is turned on, the Autodetect check box is displayed as shown in this picture. An Auto Scale automatically detects the external reference frequency. With pattern lock on, the instrument may be unable to correctly detect an external reference frequency. If this happens, clear the Autodetect check box.

PRBS data is not a suitable reference clock signal.

To ensure accuracy, the entered reference clock frequency must equal the actual external reference clock. Any deviations in either frequency will result in an inaccurate timebase. The instrument will display a warning message on the screen if the time reference is not valid. You must ensure that you connect a valid reference clock. If the precision timebase is on, you can perform an Auto Scale to reset the time reference.

Timebase Control Settings

Select Enable Precision Timebase to enable or disable the precision timebase. The Precision Timebase button's green indicator (on the button toolbar) indicates when the precision timebase is on. If any changes in the reference clock occur, click Reset Time Reference to reset the precision timebase. The time reference will fail if:

  • Reference clock signal does not meet the requirements listed above
  • A setup, in which the precision timebase was enabled when saved, is recalled
  • The instrument power is turned on, when the state of the precision timebase is enabled at instrument power off

Synchronization Method Settings

By default, precision timebase synchronization optimizes for RJ (Random Jitter) only. This provides a fast synchronization that is suitable for analysis of most signals. Optionally, you can choose to optimize both for RJ and for timebase linearity. This type of synchronization takes much longer but results in an extremely linear timebase as well as the lowest possible RJ. This type of synchronization is suggested for signals with extremely low DJ (Deterministic Jitter), where the signal rate is a multiple of the precision timebase reference frequency. For example, if your Symbol Rate is 32 GBd while your precision timebase reference frequency is 8 GHz, this option may improve the accuracy of the DJ measurements.

Status

The Status area of the dialog provides the following messages:

  • Precision Timebase Off. The precision timebase is disabled. The time reference will be invalid until the precision timebase is enabled.
  • No Time Reference. The precision timebase is enabled; however, the time reference is invalid. This status appears after changing the frequency band of the reference clock signal or recalling an instrument setup.
  • Time Reference Set. The precision timebase is enabled and the time reference is valid.
  • Time Reference Lost. The precision timebase is enabled. The instrument continues to acquire data using the most recent time reference. This status follows an absent reference clock signal, a clock signal that is too large (or too small), a clock signal that is not in a valid frequency band, or a clock signal that does not have a stable frequency.

Select the Show Precision Timebase Signals field to view the In Phase Waveform and Quadrature Waveform inputs to the precision timebase circuitry. Both an amplitude-vs-time chart and a Lissajous Pattern chart are displayed. This feature provides a qualitative view of the inputs. There is no remote command for making this selection. However, you can use the :WAVeform:SOURce command remote command to return the two waveforms.