Trigger
Instrument
N1000A
N109X
Flex Apps:
FlexDCA
Introduction
This topic describes both standard and pattern triggering of a DCA-X.
The information on triggering and pattern lock does not apply when FlexRT is enabled in FlexDCA. Triggering and pattern lock is not needed or used in FlexRT.
To Trigger the Instrument
A trigger signal must be provided to the oscilloscope using one of the following methods:
- On a DCA-X mainframe, connect a synchronous clock signal to the oscilloscope's front-panel Trigger connector. Click Setup > Trigger to open the Trigger dialog and specify Front Panel. This is the most often-used method (as well as the default) source for triggering. You can also press the instrument's front-panel Trigger Level knob to select Front Panel. After connecting and then selecting the trigger source click Auto Scale on the menu bar to set the trigger level to the amplitude midpoint of the trigger signal. To manually adjust the trigger level, turn the Trigger Level knob.
- On N109x-series DCA-M scopes, connect the clock signal to the DCA-M's front-panel Clock Trigger In connector.
- If a trigger signal is not available, use clock recovery to recover the clock. Click Setup > Trigger and select Left Module or Right Module to trigger from the clock recovery module. Compatible modules (that have front-panel trigger input connectors) include N1060A and N107x series DCA-M modules.
- Trigger on the data input to a module. Split the incoming data signal and route half of the data to the instrument's trigger input. Route the other half to the module's input connector. Due to jitter and pattern dependencies this technique shows incomplete eye diagrams and approximately 75% of waveforms are never observed in a PRBS.
- In Oscilloscope and Eye/Mask modes, you can also select Free Run. This selection causes the instrument to trigger as soon as the trigger is armed; an external trigger is not used. Free run is asynchronous to the data and can be used to quickly examine a signal's amplitude without any timing information.