Contains the settings to configure a "Cal All" Calibration.
Use the Guided Cal interface to perform the calibration.
SYSTem:CALibrate:ALL: CHANnel: CSET: | CATalog? GUIDed: | CHANnel? | PORTs? INDependent: | SOURce: | CALibrate: | CATalog? | RANGe: | ADD | CLEar | COUNt | PONts | STARt | STOP MCLass: | PROPerty: | VALue: | CATalog? | [STATe] PATH: | CONFigure: | ELEMent PORT<n>: | SOURce:POWer: | ATTen | OFFSet | [VALue]
|
Click on a red keyword to view the command details.
See Also
(Write-Read) For each channel to be calibrated, sets and returns the ports to be calibrated. Specify port numbers ONLY for standard channels. Application channels are not necessary because they have designated input/output/LO ports. |
|
Parameters |
|
<ch> |
Channel number to be calibrated. |
<value> |
Ports to be calibrated for the specified channel. Select any of the native PNA ports (1,2,3,4). |
Examples |
SYST:CAL:ALL:CHAN2:PORT 1,2,3 |
Query Syntax |
SYSTem:CALibrate:ALL:CHANnel<ch>:PORTs[:SELect]? |
Return Type |
Comma-separated port numbers. |
Default |
1,2 |
(Read-only) Returns the User Cal Set or cal register names that were produced by the cal all session. |
|
Parameters |
None |
Examples |
SYST:CAL:ALL:CSET:CATalog? 'returns this format: "MyCalAll_STD_001, MyCalAll_SMC_002" |
Return Type |
String of comma-separated Cal Set or cal register names |
Default |
Not Applicable |
(Write-Read) Sets and returns the prefix to be used when saving User Cal Sets that result from the Cal All session. The Meas Class and channel number are appended to this prefix for each calibrated channel. Use SYST:CAL:ALL:CSET:CATalog? to read the saved cal set names.
|
|
Parameters |
|
<value> |
(String) User Cal Set prefix. |
Examples |
SYST:CAL:ALL:CSET:PREFix "MyCalAll" |
Query Syntax |
SYSTem:CALibrate:ALL:CSET:PREFix? |
Return Type |
String |
Default |
" " (Empty string) |
(Read-only) Reads the channel number of the Cal All Calibration. Use this value as the <ch> argument for the subsequent Guided:Cal commands. |
|
Parameters |
None |
Examples |
chan = SYST:CAL:ALL:GUID:CHAN? |
Return Type |
Numeric |
Default |
Not applicable |
(Read-only) Returns the ports to be calibrated during the Cal All Channels calibration. Specify connectors and cal kits for these ports using the Guided:Cal commands. Specify the ports to be calibrated for each channel using SYST:CAL:ALL:CHAN<ch>:PORT. |
|
Parameters |
None |
Examples |
ports = SYST:CAL:ALL:GUID:PORT? |
Return Type |
Comma-separated list of port numbers |
Default |
Not applicable |
(Write-Read) Sets and returns the IFBW for a Cal All calibration. Learn more about this setting. |
|
Parameters |
|
<value> |
IF Bandwidth in Hz. The list of valid IF Bandwidths is different depending on the PNA model. See the list of valid settings. If an invalid number is specified, the PNA will round up to the closest valid setting. This command supports MIN and MAX as arguments. Learn more. |
Examples |
SYST:CAL:ALL:IFBW 10e3 |
Query Syntax |
SYSTem:CALibrate:ALL:IFBW? |
Return Type |
Numeric |
Default |
1 kHz |
(Read-only) Returns available ports for independent power calibration. |
|
Parameters |
None |
Examples |
SYST:CAL:ALL:IND:SOUR:CAL:CAT? |
Return Type |
String |
Default |
Not applicable |
(Write-only) This command adds a power cal range for a specific port <n>. Note that external sources are valid and specifying a source port is the same as other remote commands. By default this will create a range with the preset start/stop frequency and 201 points. The maximum number of ranges that can be added is 100 (same as the maximum number of segments). |
|
Parameters |
|
<n> |
Port number |
Examples |
SYST:CAL:ALL:IND:SOUR3:CAL:RANG:ADD |
Default |
Not applicable |
(Write-only) This command resets all ranges for the given source port <n>. |
|
Parameters |
|
<n> |
Port number |
Examples |
SYST:CAL:ALL:IND:SOUR3:CAL:RANG:CLE |
Default |
Not applicable |
(Read-only) This command queries how many ranges are included in the calibration for source port <n>. |
|
Parameters |
|
<n> |
Port number |
Examples |
SYST:CAL:ALL:IND:SOUR3:CAL:RANG:COUN? |
Return Type |
Numeric |
Default |
Not applicable |
(Write-Read) This command sets and gets the number of points for range <m> for source port<n>. |
|
Parameters |
|
<n> |
Port number |
<m> |
Range number |
<value> |
Number of points |
Examples |
SYST:CAL:ALL:IND:SOUR3:CAL:RANG1:POIN 7 |
Query Syntax |
SYSTem:CALibrate:ALL:INDependent:SOURce<n>:CALibrate:RANGe<m>:POINts? |
Return Type |
Numeric |
Default |
Not applicable |
(Write-Read) This command sets and gets the start frequency for range <m> for source port<n>. |
|
Parameters |
|
<n> |
Port number |
<m> |
Range number |
<value> |
Start frequency for range <m> |
Examples |
SYST:CAL:ALL:IND:SOUR3:CAL:RANG1:STAR 20e9 |
Query Syntax |
SYSTem:CALibrate:ALL:INDependent:SOURce<n>:CALibrate:RANGe<m>:STARt? |
Return Type |
Numeric |
Default |
Not applicable |
(Write-Read) This command sets and gets the stop frequency for range <m> for source port<n>. |
|
Parameters |
|
<n> |
Port number |
<m> |
Range number |
<value> |
Stop frequency for range <m> |
Examples |
SYST:CAL:ALL:IND:SOUR3:CAL:RANG1:STOP 21e9 |
Query Syntax |
SYSTem:CALibrate:ALL:INDependent:SOURce<n>:CALibrate:RANGe<m>:STOP? |
Return Type |
Numeric |
Default |
Not applicable |
(Read-only) Returns the unique, settable properties for the current cal all session. See a list of valid properties and values for each measurement class. |
|
Parameters |
|
[mclass] |
Optional argument. String name of the measurement class for which properties are to be returned. See a list of valid measurement class Application names. The measurement class must be included in the current Cal All calibration. |
Examples |
SYST:CAL:ALL:MCL:PROP:NAME:CAT? 'with NFX app, returns: "Noise Cal Method,Noise Tuner,AutoOrient Tuner,Tuner In,Tuner Out,Receiver Characterization Method,ENR File,Noise Source Connector,Noise Source CalKit" |
Return Type |
String of comma-separated properties. |
Default |
Not applicable |
(Read-only) Returns the valid property values for a specific property name. See a list of valid properties and values for each measurement class. |
|
Parameters |
|
<prop> |
(String) Property name for which valid values are to be returned. |
Examples |
SYST:CAL:ALL:MCL:PROP:VAL:CAT? "Noise Cal Method" 'with NFX app, returns: "Scalar,Vector" |
Return Type |
String of comma-separated values |
Default |
Not applicable |
(Write-Read) Sets and returns the property value for a specific property name. See a list of valid properties and values for each measurement class. |
|
Parameters |
|
<prop> |
(String) Property name for which value is to be set or returned. |
<value> |
Property value. To read a list of valid values, use SYST:CAL:ALL:MCL:PROP:VAL:CAT? |
Examples |
Example
1: Example 2: Example 3: |
Query Syntax |
SYSTem:CALibrate:ALL:MCLass:PROPerty:VALue[:STATe]? <prop> |
Return Type |
String |
Default |
Varies with the property name. |
(Write-Read) Sets and returns the Path Configuration settings for a Cal All calibration. |
|
Parameters |
|
<element> |
(String) Path configuration element to be set. See a list of configurable RF Path elements and settings. |
<setting> |
(String) Path configuration element setting. |
Examples |
SYST:CAL:ALL:PATH:CONFigure:ELEMent "Port1NoiseTuner","Internal" |
Query Syntax |
SYSTem:CALibrate:ALL:PATH:CONFigure:ELEMent[:STATe]? <element> |
Return Type |
String |
Default |
Not Applicable |
(Write-Read) Sets and returns the Receiver Attenuator setting for a Cal All calibration. |
|
Parameters |
|
<n> |
Receiver port number. |
<value> |
Attenuation value in dB for a Cal All calibration. Choose a valid value for the PNA model. See valid settings. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SYST:CAL:ALL:PORT2:REC:ATT 10 |
Query Syntax |
SYSTem:CALibrate:ALL:PORT<n>:RECeiver:ATTen? |
Return Type |
Numeric |
Default |
0 |
(Write-Read) Sets and returns the Source Attenuator setting for the Cal All calibration. |
|
Parameters |
|
<n> |
Source port number. |
<value> |
Attenuation value in dB for the Cal All calibration. Choose a valid value for the PNA model. See valid settings. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SYST:CAL:ALL:PORT2:SOUR:POW:ATT 10 |
Query Syntax |
SYSTem:CALibrate:ALL:PORT<n>:SOURce:POWer:ATTen? |
Return Type |
Numeric |
Default |
0 |
(Write-Read) Sets and returns the power offset value for a Cal All calibration. Power Offset provides a method of compensating port power for added attenuation or amplification in the source path. The result is that power at the specified port reflects the added components. |
|
Parameters |
|
<n> |
Source port number. |
<value> |
Power offset value in dB for a Cal All calibration.
|
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SYST:CAL:ALL:PORT2:SOUR:POW:OFFS 10 |
Query Syntax |
SYSTem:CALibrate:ALL:PORT<n>:SOURce:POWer:OFFSet? |
Return Type |
Numeric |
Default |
0 |
(Write-Read) Sets and returns the power level at which a Cal All calibration is to be performed. |
|
Parameters |
|
<n> |
Source port number. |
<value> |
Power level at which the calibration is to be performed. |
[src] |
String. (NOT case sensitive). Source port. Optional. Use SOUR:CAT? to return a list of valid port names. While this argument can be used to make settings for ALL ports, it is designed to access ports such as an external source, true mode balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model such as "Port 1 Src2". Otherwise, the <port> argument performs the same function. If both arguments are specified, [src] takes priority. |
Examples |
SYST:CAL:ALL:PORT2:SOUR:POW 0 |
Query Syntax |
SYSTem:CALibrate:ALL:PORT<n>:SOURce:POWer[:VALue]? |
Return Type |
Numeric |
Default |
Preset power of the PNA model. |
(Write-only) Resets all properties associated with the Cal All session to their default values. |
|
Parameters |
None |
Examples |
SYST:CAL:ALL:RES |
Query Syntax |
Not Applicable |
Default |
Not Applicable |
(Write-Read) Sets and returns the list of channels to be calibrated during the Cal All session. |
|
Parameters |
|
<value> |
Channel numbers to be calibrated. These channels must already exist. |
Examples |
SYST:CAL:ALL:SEL 1,2,3 |
Query Syntax |
SYSTem:CALibrate:ALL:SELect? |
Return Type |
Comma-separated channel numbers. |
Default |
Existing channels |