:CALibrate:PROBe:CHANnel:ENABled

Command Syntax

:CALibrate:PROBe:CHANnelN:ENABled {ENABled | DISabled}

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CALibrate:PROBe:CHANnelN:ENABled?

Description

On the indicated channel, enables/disables the all the probe's calibrations (Vertical, Skew, and AC Response).

To enable or disable the probe's calibrations individually, see :CALibrate:PROBe:CHANnel:VERTical:ENABled and :CALibrate:PROBe:CHANnel:SKEW:ENABled.

To run all enabled probe calibrations, see :CALibrate:PROBe:CHANnel:STARt.