:CALibrate:PROBe:CHANnel:SKEW:STATus:DETails?

Query Syntax

:CALibrate:PROBe:CHANnelN:SKEW:STATus:DETails?

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Description

Queries a string of status details for the Skew Adjustment status for the probe on the specified channel.

Parent Command