:CALibrate:PROBe:CHANnel:VERTical:STATus:TIME?

Query Syntax

:CALibrate:PROBe:CHANnelN:VERTical:STATus:TIME?

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Description

For the probe on the specified channel, determines the oldest date and time between the last vertical calibration and returns the value.

If an adjustment has not yet been performed, an empty string is returned.

Parent Command