:CALibrate:PROBe:CHANnel:STATus:DETails?

Query Syntax

:CALibrate:PROBe:CHANnelN:STATus:DETails?

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Description

Queries a string of status details for all calibrations for the probe on the specified channel. The following is an example of a typical returned string:

Time of last Calibration: 10/23/2012 11:52:00,Elapsed Calibration Time: 3 hours 2 minutes,Temperature Change: 1.24 C"

If a calibration is recommended, the following text is placed at the beginning of the above string:

"Requires Calibration, …"

If a calibration has not yet been performed, the following string is returned:

"This calibration has never been performed in this instrument."

Parent Command