:CALibrate:PROBe:CHANnel:STATus:TIME?
Query Syntax
:CALibrate:PROBe:CHANnelN:STATus:TIME?
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Description
For the probe on the specified channel, determines the oldest date and time between the last vertical calibration or skew calibration and returns the value. If a calibration has not yet been performed, an empty string is returned.
Example Returned Status String
"03/22/2026 14:52:00"