:CALibrate:PROBe:CHANnel:VERTical:ENABled

Command Syntax

:CALibrate:PROBe:CHANnelN:VERTical:ENABled {ENABled | DISabled}

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CALibrate:PROBe:CHANnelN:VERTical:ENABled?

Description

On the indicated channel, enables/disables the all the probe's vertical calibration.

To enable or disable the other individual probe's calibrations, see :CALibrate:PROBe:CHANnel:SKEW:ENABled.

To enable or disable all the probe's calibrations, see :CALibrate:PROBe:CHANnel:ENABled.

To run all enabled probe calibrations, see :CALibrate:PROBe:CHANnel:STARt.