:CALibrate:PROBe:CHANnel:STARt

Command Syntax

:CALibrate:PROBe:CHANnelN:STARt

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Description

On the indicated channel, runs all enabled calibrations in the order: Vertical, Skew, AC Response.

To enable or disable all probe calibrations, see :CALibrate:PROBe:CHANnel:ENABled.

To enable or disable individual probe calibrations, see :CALibrate:PROBe:CHANnel:VERTical:ENABled, :CALibrate:PROBe:CHANnel:SKEW:ENABled.

The *OPC (Operation Complete) query should be used to detect when a portion of the calibration has completed.

Use the :CALibrate:CONTinue command to dismiss dialog boxes that are displayed during a calibration.

Example Command Sequence

:CALibrate:PROBe:CHANnel3:STARt
*OPC?
…  //  Your code to synchronize execution timing.
:CALibrate:CONTinue
*OPC?
…  //  Your code to synchronize execution timing.
:CALibrate:CONTinue