:CALibrate:PROBe:CHANnel:STATus?
Query Syntax
:CALibrate:PROBe:CHANnelN:STATus?
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Description
Queries the overall calibration status for the probe on the specified channel. If a vertical or skew calibration is needed, the probe on the specified channel is considered to be uncalibrated.
One of the following response strings is returned:
- "CALIBRATED"
- The calibrations are valid.
- "UNCALIBRATED"
- At least one calibration is needed.
- ""
- An empty string is returned if the hardware for the indicated connection number does not exist. An -241,"Hardware missing" error is returned by the
:SYSTem:ERRor:NEXT?command.
To check the status of the individual calibrations, use the :CALibrate:PROBe:CHANnel:VERTical:STATus? or :CALibrate:PROBe:CHANnel:SKEW:STATus? queries.
Use the child queries listed in the following table to return details about the current calibration.
| Status String | Child Query to Send |
|---|---|
| Time of last calibration, Time change since last calibration, and Temperature change since last calibration |
:CALibrate:PROBe:CHANnel:STATus:DETails?
|
| Change in temperature | :CALibrate:PROBe:CHANnel:STATus:DTEMperature?
|
| Change in Time | :CALibrate:PROBe:CHANnel:STATus:TIME?
|