:CHANnel:UNAMe
Command Syntax
:CHANnelN:UNAMe <string>
{N} identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:UNAMe?
Description
Assigns a custom user name to a channel waveform. User names are helpful because they identify what a waveform represents rather than the oscilloscope's input channel. For example, you could assign user name "DUT 18, Lane 4" to connection 1 channel 2's waveform. User names can be 25 characters or less and are displayed on the screen and on screen captures. To remove a custom user name, re-create it using an empty string.
Custom user names can by created for other waveforms using the following commands:
Example Command Sequence
:CHANnel1_2:UNAMe "DUT 18, Lane 4"