:WMEMory:UNAMe

Command Syntax

:WMEMoryN:UNAMe <string>

{1:8} identifies one of eight waveform memories. For example, the memory 2 would be identified as :WMEMory2

Query Syntax

:WMEMoryN:UNAMe?

Description

Assigns a custom user name to waveform memory. User names are helpful because they identify what a waveform represents rather than the oscilloscope's input channel. For example, you could assign user name "DUT Output" to the memory 2 waveform. User names can be 25 characters or less and are displayed on the screen and on screen captures. To remove a custom user name, re-create it using an empty string. To assign the user name to the name of the waveform file that was imported into color grade memory, use the :WMEMory:UNAMe:UFName command.

Custom user names can by created for other waveforms using the following commands:

Example Command Sequence

:WMEMory4:UNAMe "DUT Output"