:FUNCtion:CRECovery:ECLock:EDIRection
:FUNCtion CRECovery Commands
- :FUNCtion CRECovery Commands
- :FUNCtion:CRECovery:CEALgorithm
- :FUNCtion:CRECovery:CEIDle
- :FUNCtion:CRECovery:CFRequency:EDIRection
- :FUNCtion:CRECovery:CFRequency:MODE
- :FUNCtion:CRECovery:CSKew
- :FUNCtion:CRECovery:CSRate?
- :FUNCtion:CRECovery:DDRFive:CAFLatency
- :FUNCtion:CRECovery:DDRFive:CAFSource
- :FUNCtion:CRECovery:DDRFive:DQSSource
- :FUNCtion:CRECovery:DDRFive:POLength
- :FUNCtion:CRECovery:DDRFive:PRLength
- :FUNCtion:CRECovery:DDRFive:RWMode
- :FUNCtion:CRECovery:DDRFive:STDDelay
- :FUNCtion:CRECovery:DREMoval
- :FUNCtion:CRECovery:ECLock:ALIGn
- :FUNCtion:CRECovery:ECLock:CFRequency
- :FUNCtion:CRECovery:ECLock:CMULtiplier
- :FUNCtion:CRECovery:ECLock:DELay
- :FUNCtion:CRECovery:ECLock:EDIRection
- :FUNCtion:CRECovery:ECLock:SOURce
- :FUNCtion:CRECovery:FOPLl:LBANdwidth
- :FUNCtion:CRECovery:FOPLl:LBDivisor
- :FUNCtion:CRECovery:FSRate
- :FUNCtion:CRECovery:ICCount
- :FUNCtion:CRECovery:MODE
- :FUNCtion:CRECovery:PLL:EDIRection
- :FUNCtion:CRECovery:PLL:MODE
- :FUNCtion:CRECovery:PLL:SSCCorrect
- :FUNCtion:CRECovery:PLL:SSPercent
- :FUNCtion:CRECovery:PLL:SSType
- :FUNCtion:CRECovery:PLL:STIMe
- :FUNCtion:CRECovery:PLL:TDEPendent
- :FUNCtion:CRECovery:PRESets
- :FUNCtion:CRECovery:PRESets:SELections?
- :FUNCtion:CRECovery:SOPLl:JTF:LBANdwidth
- :FUNCtion:CRECovery:SOPLl:JTF:LBDivisor
- :FUNCtion:CRECovery:SOPLl:JTF:PEAKing
- :FUNCtion:CRECovery:SOPLl:OJTF:DFACtor
- :FUNCtion:CRECovery:SOPLl:OJTF:LBANdwidth
- :FUNCtion:CRECovery:SOPLl:OJTF:LBDivisor
- :FUNCtion:CRECovery:SRATe
- :FUNCtion:CRECovery:SRATe:STATus?
- :FUNCtion:CRECovery:SRATe:STATus:DETails?
- :FUNCtion:CRECovery:SRATe:STATus:REASon?
- :FUNCtion:CRECovery:TOPLl:DFACtor
- :FUNCtion:CRECovery:TOPLl:NFReq
- :FUNCtion:CRECovery:TOPLl:PFReq
- :FUNCtion:CRECovery:TRACking
- :FUNCtion:CRECovery:ZOPLl:LFPole
- :FUNCtion:CRECovery:ZOPLl:PPOLe
- :FUNCtion:CRECovery:ZOPLl:SPOLe
Command Syntax
:FUNCtionN:CRECovery:ECLock:EDIRection {RISing | FALLing | BOTH}
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtionN:CRECovery:ECLock:EDIRection?
Description
Specifies the edge(s) used in the explicit clock.
Example Command Sequence
:FUNCtion1:CRECovery:MODE ECLock :FUNCtion1:CRECovery:ECLock:EDIRection BOTH