:FUNCtion:CRECovery:ICCount

Command Syntax

:FUNCtionN:CRECovery:ICCount <idle_clock_count>

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

<idle_clock_count> is an integer from 10 to 200.

Query Syntax

:FUNCtionN:CRECovery:ICCount?

Description

When Contains Electrical Idle is enabled (see :FUNCtion:CRECovery:CEIDle), this command specifies the number of clock periods without a data transition (edge) that indicate an idle condition. This option lets protocol decoders suppress decode for idle data periods on serial data links that go quiescent for a period of time and then restart transmitting.

Example Command Sequence

:FUNCtion1:CRECovery:MODE FOPLl
:FUNCtion1:CRECovery:CEIDle ON
:FUNCtion1:CRECovery:ICCount 80