:FUNCtion:CRECovery:SOPLl:OJTF:DFACtor
Command Syntax
:FUNCtionN:CRECovery:SOPLl:OJTF:DFACtor <damping_factor>
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
<damping_factor> is a double.
Query Syntax
:FUNCtionN:CRECovery:SOPLl:OJTF:DFACtor?
Description
When specifying the PLL's loop bandwidth in terms of the OJTF 3 dB BW, you also need to specify the damping factor of the JTF.
| < 1 | underdamped |
| > 1 | overdamped |
| = 1.0 | critically damped |
| = 0.707 | Often considered ideal or optimal because of its fast settling time (optimally flat) and Butterworth type response. |
Example Command Sequence
:FUNCtion1:CRECovery:MODE SOPLl :FUNCtion1:CRECovery:PLL:MODE OJTF :FUNCtion1:CRECovery:SOPLl:OJTF:LBDivisor 1.670E+3 :FUNCtion1:CRECovery:SOPLl:OJTF:DFACtor 0.707