:FUNCtion:CRECovery:SOPLl:JTF:PEAKing

Command Syntax

:FUNCtionN:CRECovery:SOPLl:JTF:PEAKing <peaking_in_dB>
            

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

<peaking_in_dB> is a double.

Query Syntax

:FUNCtionN:CRECovery:SOPLl:JTF:PEAKing?

Description

When specifying the PLL's loop bandwidth in terms of the JTF 3 dB BW, you also need to specify the peaking of the JTF.

Example Command Sequence

:FUNCtion1:CRECovery:MODE SOPLl
:FUNCtion1:CRECovery:PLL:MODE JTF
:FUNCtion1:CRECovery:SOPLl:JTF:LBDivisor 1.047E+3
:FUNCtion1:CRECovery:SOPLl:JTF:PEAKing 1.25