:FUNCtion:CRECovery:PLL:MODE
Command Syntax
:FUNCtionN:CRECovery:PLL:MODE {JTF | OJTF}
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtionN:CRECovery:PLL:MODE?
Description
Chooses whether whether to specify the PLL's response in terms of either the JTF's 3 dB bandwidth and its peaking or the OJTF's 3 dB bandwidth and its damping factor.
-
JTF(Jitter Transfer Function) — This is the closed-loop transfer function of the PLL. It is the ratio of the jitter on the PLL's output clock to the jitter on the input signal.This function generally has a low-pass effect. That is, JTF is at unity over low frequencies, but as the jitter increases to higher frequencies, the jitter on the recovered clock will decrease in magnitude.
Use the
:FUNCtion:CRECovery:SOPLl:JTF:PEAKingcommand to specify the peaking of the JTF. -
OJTF(Observed Jitter Transfer Function, sometimes referred to as the Error Function) — This is the jitter between the PLL's input signal and PLL's output clock. It is equivalent to the PLL's Error Function (OJTF = EF = 1 – JTF).This function generally has a high-pass effect. That is, OJTF is at unity over high frequencies, but as the jitter decreases to lower frequencies, the jitter on the displayed waveform will decrease in magnitude.
Use the
:FUNCtion:CRECovery:SOPLl:OJTF:DFACtorcommand to specify the damping factor of the JTF.
Example Command Sequence
:FUNCtion1:CRECovery:MODE SOPLl :FUNCtion1:CRECovery:PLL:MODE JTF :FUNCtion1:CRECovery:SOPLl:JTF:LBANdwidth 2.837E+6 :FUNCtion1:CRECovery:SOPLl:JTF:PEAKing 1.25