:FUNCtion:CRECovery:SRATe:STATus:DETails?
Query Syntax
:FUNCtionN:CRECovery:SRATe:STATus:DETails?
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Response
Refer to the table "Common Reasons for INV or QUES Status".
Description
If the status of the clock recovery symbol rate is questionable or invalid (see :FUNCtion:CRECovery:SRATe:STATus?), this query returns a string that may provide additional details.
If the status of the clock recovery symbol rate is valid, this query returns an empty string.
For a basic reason for the questionable or invalid status, use the :FUNCtion:CRECovery:SRATe:STATus:REASon? sibling query.