:FUNCtion:CRECovery:PLL:SSCCorrect
Command Syntax
:FUNCtionN:CRECovery:PLL:SSCCorrect {ON | OFF | 1 | 0}
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtionN:CRECovery:PLL:SSCCorrect?
Description
Lets you enable or disable the application of SSC (spread-spectrum clocking) correction. This information improves the performance of clock recovery.
When enabled:
-
Use the
:FUNCtion:CRECovery:PLL:SSTypecommand to specify the type of SSC being used. -
Use the
:FUNCtion:CRECovery:PLL:SSPercentcommand to specify the magnitude of the symbol rate change (spread) as a percent.