:FUNCtion:CRECovery:SRATe:STATus?
Query Syntax
:FUNCtionN:CRECovery:SRATe:STATus?
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Response
{CORR | INV | QUES}
- CORR
- The measurement result is correct.
- INV
- The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
- QUES
- The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.
Description
Queries the status of the :FUNCtion:CRECovery:SRATe measurement. Use the :FUNCtion:CRECovery:SRATe:STATus:REASon? child query to determine the reason for an invalid or questionable measurement