:FUNCtion:CRECovery:SRATe:STATus:REASon?
Query Syntax
:FUNCtionN:CRECovery:SRATe:STATus:REASon?
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Response
Refer to the table "Common Reasons for INV or QUES Status".
Description
Returns a string that explains the reason for a failed :FUNCtion:CRECovery:SRATe measurement. If the measurement was successful, a null string is returned.
Use the :FUNCtion:CRECovery:SRATe:STATus? parent query to determine if the measurement has failed.