:PROTocol:PROTocol:STATus?
Query Syntax
:PROTocol:PROTocolN:STATus?
Where N identifies one of four possible protocol decodes {1:4}. For example, PROTocol3.
Query Response
{CORR | INV | QUES}
- CORR
- The measurement result is correct.
- INV
- The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
- QUES
- The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.
Description
Status of the protocol results (Invalid, Correct, Questionable)
Queries the status of the protocol decode. Use the :PROTocol:PROTocol:STATus:REASon? child query to determine the reason for an invalid or questionable measurement. Additional information about the failure may be available using the :PROTocol:PROTocol:STATus:DETails? child query.