:NETWorks:TRACe:XPOSition?

Query Syntax

:NETWorks:TRACeN:XPOSition?

Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.

Description

Queries the value at the center of the X-axis for the graph of the indicated S-parameter trace. Use the :NETWorks:TRACe:XSCale? command to query the scale of the horizontal axis. Query the value at the left side of the graph using the :NETWorks:TRACe:XLEFt? command. Query the value at the ride side of the graph using the :NETWorks:TRACe:XRIGht? command.

Units for Displayed Content Window Graphs
Content Window Graphs Y-Axis
Units
X-Axis
Units
S-Parameters
Freq-Mag Decibels Hertz
Phase Degrees
GrpDelay Seconds