:NETWorks:TRACe:YBOTtom?

Query Syntax

:NETWorks:TRACeN:YBOTtom?

Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.

Description

Queries the Y-axis value at the bottom of the graph for the indicated S-parameter trace. Use the :NETWorks:TRACe:YUNits? command to return the units-of-measurement. Use the :NETWorks:TRACe:OPERator command to return the type of graph and the :NETWorks:TRACe:PARameter command to return the actual S-parameter viewed.