:NETWorks:TRACe:XREFerence?

Query Syntax

:NETWorks:TRACeN:XREFerence?

Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.

Description

Returns the X-axis reference point on the indicated S-parameter trace. The value returned is CENT which stands for the center of the axis.