:NETWorks:TRACe:XLEFt?
Query Syntax
:NETWorks:TRACeN:XLEFt?
Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.
Description
Queries the X-axis value at the left edge of the graph for the indicated S-parameter trace. Use the :NETWorks:TRACe:XSCale? query to return the scale. Use the :NETWorks:TRACe:XUNits? command to return the units-of-measurement. Use the :NETWorks:TRACe:OPERator command to return the type of graph and the :NETWorks:TRACe:PARameter command to return the actual S-parameter viewed.