:NETWorks:TRACe:YSCale?

Query Syntax

:NETWorks:TRACeN:YSCale?

Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.

Description

Queries the Y-axis scale for the graph of the indicated S-parameter trace. Use the :NETWorks:TRACe:YOFFset? command to set or query the value at the center of the vertical axis. You can query the value at the top of the graph using the :NETWorks:TRACe:YTOP? command. You can query the value at the bottom of the graph using the :NETWorks:TRACe:YBOTtom? command.

Units for Displayed Content Window Graphs
Content Window Graphs Y-Axis
Units
X-Axis
Units
S-Parameters
Freq-Mag Decibels Hertz
Phase Degrees
GrpDelay Seconds