:NETWorks:TRACe:YUNits?
Query Syntax
:NETWorks:TRACeN:YUNits?
Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.
Query Response
{OHM | VOLT | PERC | DEGR | SEC | DEC}
Description
Queries the Y-axis units-of-measurement for the indicated S-parameter trace. The returned strings are described in the following table.
| Returned String |
Y-Axis Units |
Content Window Graphs |
|---|---|---|
| S-Parameters | ||
| DEC | Decibels | Freq-Mag |
| DEGR | Degrees | Phase |
| SEC | Seconds | GrpDelay |