:NETWorks:TRACe:XSCale?
Query Syntax
:NETWorks:TRACeN:XSCale?
Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.
Description
Queries the X-axis scale for the graph of the indicated S-parameter trace. Use the :NETWorks:TRACe:XPOSition? command to set or query the value at the center of the horizontal axis. You can query the value at the left side of the graph using the :NETWorks:TRACe:XLEFt? command. You can query the value at the ride side of the graph using the :NETWorks:TRACe:XRIGht? command.
| Content Window Graphs | Y-Axis Units |
X-Axis Units |
|---|---|---|
| S-Parameters | ||
| Freq-Mag | Decibels | Hertz |
| Phase | Degrees | |
| GrpDelay | Seconds | |