:NETWorks:TRACe:XRIGht?

Query Syntax

:NETWorks:TRACeN:XRIGht?

Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.

Description

Queries the X-axis value at the right edge of the graph for the indicated S-parameter trace. Use the :NETWorks:TRACe:XSCale? command to return the units-of-measurement. Use the :NETWorks:TRACe:XUNits? command to return the units-of-measurement. Use the :NETWorks:TRACe:OPERator command to return the type of graph and the :NETWorks:TRACe:PARameter command to return the actual S-parameter viewed.