:NETWorks:TRACe:XUNits?
Query Syntax
:NETWorks:TRACeN:XUNits?
Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.
Query Response
{HERT}
Description
Queries the X-axis units-of-measurement for the indicated S-parameter trace. The units for S-parameters is Hertz which is indicated with the returned HERT string.
| Returned String |
X-Axis Units |
Content Window Graphs |
|---|---|---|
| S-Parameters | ||
| HERT | Hertz | Freq-Mag |
| Phase | ||
| GrpDelay |