:NETWorks:TRACe:YRANge?

Query Syntax

:NETWorks:TRACeN:YRANge?

Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.

Description

Queries the trace graph's vertical range (sensitivity). This is the vertical scale per division value (:NETWorks:TRACe:YSCale?) multiplied by eight divisions.

Use the :NETWorks:TRACe:YOFFset? command to set or query the value at the center of the vertical axis.

You can query the value at the top of the graph using the :NETWorks:TRACe:YTOP? command.

You can query the value at the bottom of the graph using the :NETWorks:TRACe:YBOTtom? command.

Units for Displayed Content Window Graphs
Content Window Graphs Y-Axis
Units
X-Axis
Units
S-Parameters
Freq-Mag Decibels Hertz
Phase Degrees
GrpDelay Seconds