:SYSTem:AENable
Command Syntax
:SYSTem:AENable {ON | OFF | 1 | 0}
Query Syntax
:SYSTem:AENable?
Description
This command lets you select or clear the Allow Analysis control in the user interface which prevents or allows analysis.
Preventing analysis lets you make a sequence of settings and configuration changes more quickly because analysis will not restart with each change.
Query Response
{1 | 0}