:SYSTem:FUNCtions:REMove

Command Syntax

:SYSTem:FUNCtions:REMove

Description

Removes all math functions from the analysis graph. This is not just turning the math function displays off.

While there is no SCPI command to restore all math functions, you can undo this action by clicking Setup > Undo from Infiniium's front panel. Or, you can recreate your math functions using the commands in the :FUNCtion Subsystem subsystem.