:SYSTem:MENU:APPLications:LAUNch
Command Syntax
:SYSTem:MENU:APPLications:LAUNch "<string>"
<string> is the name of an installed real-time oscilloscope compliance application.
Description
Launches a real-time oscilloscope compliance application. Installed applications appear on the Tools > Apps > Automated Test Apps menu.
You can get a comma-separated list of the installed compliance applications using the :SYSTem:MENU:APPLications? query.
Another way to find the appropriate string for launching a compliance application is turn on the graphical user interface's SCPI Recorder and start the application from the GUI menu.