Location of Files
These folders are the default locations for saving specific types of files. For example, screen capture files that you save are, by default, saved in the \Screen Images subfolder. You can always save files to any folder that you wish including those on a network or external drive.
To protect you user files, it is recommended that you backup this folder to an external or network drive.
The following subfolders exist under the %USER_DATA_DIR% folder:
- Adapter Definitions
- Colorgrade-Grayscale
- De-Embedding Networks
- Documentation Results
- Jitter Data
- Limit Lines
- Limit Summaries
- Masks
- Patterns
- Presets
- ClockRecovery
- CTLE
- DFE
- ElectricalSIRC
- FFE
- JitterThresholds
- RandomOperator
- Protocols
- SCPI Scripts
- Screen Images
- Setups
- SNDR
- S-Parameter Data
- User App Menu Items
- User Functions
- User Measurements
- Waveforms
| Subfolder | Contents | Remote Commands |
|---|---|---|
| Adapter Definitions | . | : |
| Colorgrade-Grayscale | Saved eye-mode database files (.cgsi) that usually contain eye-diagram data. These files can be loaded into eye memory. | :DISK:EYE:SAVE
:CGMemory:FILE:LOAD |
| De-Embedding Networks | Saved de-embedding network files (.tf4) files created using function's 2-port and 4-port de-embedding operators. Using remote programming commands, you can load but cannot create and define networks. | :FUNCtion:PARameters:DEMBed:FNAMe
:FUNCtion:PARameters:DDEMbed:FNAMe |
| Documentation Results | Saved Documentation Wizard report files (.zip). Documentation files can be configured and saved from the GUI. Remotely, they can be configured but not saved. | :DISK:DWIZard:FNAMe |
| Limit Lines | Saved limit line definitions. | :LLINe:LOAD:FNAMe |
| Limit Summaries | Saved Summary Report files (.sum) from limit line limit testing. | :LTESt:LLINe:SSUMmary:FNAMe |
| Masks | Supplied or modified eye-mode mask definition files (.mskx, .msk). These files can be loaded. | :MTESt:LOAD |
| Presets | Saved mini-setup files for: | |
| Clock Recovery Configuration. | :CRECovery:PRESets | |
| DFE (Decision Feedback Equalizer) Operator configuration. | :FUNCtion:PARameters:DFEQualizer:PRESets | |
| Continuous Time Linear Equalizer Operator configuration. | :FUNCtion:PARameters:CTLequalizer:PRESets | |
| Linear Equalizer Operator configuration | :FUNCtion:PARameters:FFEQualizer:PRESets | |
| Presets | Saved mini-setup files of the following types. Presets can only be saved from dialogs and not programmatically. | |
| CDR Presets. Saved from the Receiver tab of the System Setup dialog. | :CRECovery:PRESets | |
| Source Presets. Saved from the Source tab of the System Setup dialog. | :CRECovery:PRESets | |
| System Presets. | :CRECovery:PRESets | |
| SCPI Scripts | Saved recorded SCPI scripts (.scpi) that can be loaded and saved | :SYSTem:MPButton:FUNCtion |
| Screen Images | Saved image files of the screen. | :DISK:SIMage:SAVE |
| Setups | Saved instrument setups. | :DISK:SETup:SAVE
:DISK:SETup:RECall |
| S-Parameter Data | Saved S-parameters Touchstone files. | :DISK:DWIZard:SSParam :DISK:DWIZard:SAVE |
| User App Menu Items | Place your own custom file and PC application shortcuts in this folder. These items will automatically appear on Infiniium's Apps menu. | none |
| User Measurements | User-defined measurements. Can be defined from Matlab or Python scripts. | :MEASure:EYE:USER:USER:CFILe
:MEASure:USER:USER:CFILe |
| Waveforms | Saved oscilloscope-mode single-valued waveforms. | :DISK:WAVeform:SAVE
:WMEMory:LOAD |