Baseband Studio for waveform capture and playback has a variety of uses. Some of the more common uses include baseband modem test, hybrid component test, and predistortion loop calibration. This section provides the following basic setup examples. Use them in different combinations to suit your test and verification needs.
Basic Capture Setup - Capture digital IQ baseband data from a DUT to the Agilent 89600 Vector Signal Analyzer software and to a PC file.
Basic Digital IQ Playback Setup - Play digital IQ baseband data from a PC file directly to a DUT.
Basic RF Playback Setup - Play digital IQ baseband data from a PC file to an ESG or PSG, then to a DUT as an RF signal or as analog IQ.
Playback Setup with Dual N5101A PCI Cards - Play digital or RF waveforms from a PC file to two ESGs/PSGs or two DSIMs while running two instances of the N5110B software.
This section also contains the following informational topics: