:CALibrate:FRAMe:TIMebase:USER:EXPort
Instruments:
N1000A
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:CALibrate:FRAMe:TIMebase:USER:EXPort "filename.cal"
Description
Allows you to export the calibration data from a N1000A User Timebase Calibration as an XML file (*.xml). This may be useful if you operate your instrument at several different temperatures, and you wish to save a calibration for each temperature. To import the data back into the N1000A, use the :CALibrate:FRAMe:TIMebase:USER:IMPort command.
Requires FlexDCA revision A.06.00 and above.