:CALibrate:FRAMe:TIMebase:USER:STATus?
Instruments:
N1000A
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CALibrate:FRAMe:TIMebase:USER:STATus?
Query Response
{CALIBRATED | UNCALIBRATED}
Description
Returns the status of an DCA-X's user timebase calibration. Use the :CALibrate:FRAMe:TIMebase:USER:STATus:DETails?, :CALibrate:FRAMe:TIMebase:USER:STATus:DTEMperature?, and :CALibrate:FRAMe:TIMebase:USER:STATus:TIME? child queries to return detailed information about the calibration status. To run the calibration, use the :CALibrate:FRAMe:TIMebase:USER:STARt command.
Requires FlexDCA revision A.05.80 and above.