:CALibrate:FRAMe:TIMebase:USER:STATus:DTEMperature?
Instruments:
N1000A
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CALibrate:FRAMe:TIMebase:USER:STATus:DTEMperature?
Query Response
<delta temperature>
Description
Returns a number that provides the change in temperature (Celsius) of the Mainframe User Timebase calibration since the last calibration. Use the :CALibrate:FRAME:TIMebase:USER:STATus? parent query to determine if a calibration is needed. Use the :CALibrate:FRAME:TIMebase:USER:STARt command to calibrate the timebase.
Example of Returned Status String
8.13E+00
Requires FlexDCA revision A.05.80 and above.