:CALibrate:FRAMe:TIMebase:USER:STATus:TIME?
Instruments:
N1000A
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CALibrate:FRAMe:TIMebase:USER:STATus:TIME?
Query Response
"<time>"
Description
Returns a string that provides the time that has elapsed since the last Mainframe User Timebase calibration. Use the :CALibrate:FRAME:TIMebase:USER:STATus? parent query to determine if a calibration is needed. Use the :CALibrate:FRAME:TIMebase:USER:STARt command to calibrate the timebase.
Examples of Returned Status Strings
"10/08/2018 15:01:32"
"UNKNOWN"
Requires FlexDCA revision A.05.80 and above.