:CALibrate:FRAMe:TIMebase:USER:STARt
Command Syntax
:CALibrate:FRAMe:TIMebase:USER:STARt
Description
Starts an N1000A mainframe user calibration. The following table lists the input clock signal requirements for the calibration waveform. The source of the calibration waveform must be a calibrated microwave or vector signal generator. Do not use a pattern generator or arbitrary waveform generator. When the calibration starts, the N1000A automatically switches to oscilloscope mode.
Connect the signal to an N1000A's electrical channel input and to the front-panel trigger input. Use the :CALibrate:FRAMe:TIMebase:USER:CHANnel command to specify the input channel. After performing the calibration, you can export the calibration data to an xml file using the :CALibrate:FRAMe:TIMebase:USER:EXPort command. The file can be imported back into the N1000A.
| DCA-X | Frequency | Amplitude |
|---|---|---|
| N1000A | 26.000000 GHz | 140 mVpp to 980 mVpp |
Requires FlexDCA revision A.05.80 and above.